Hvordan kan vi hjælpe dig i dag?

Video: How to change the type of stop on an ATS48 from freewheel to ramp stop?

Issue:
Stop type configuration ATS48

Product Line:
Altistart 48 series soft starters.

Environment:
All makes, All models

Cause:
Customer needs a ramp stop to allow a check valve to close slowly to prevent water hammering.

Resolution:
Under the Settings Menu (Set) set parameter STY to D to select a deceleration stop type.
Under the Settings Menu (Set) set parameter DEC to the time, in seconds, that you want the starter to take to bring the motor to a stop after the run command is removed.