Hvordan kan vi hjælpe dig i dag?

Power Monitoring Expert Diagnostics Tool fails on every command

Issue:
The Power Monitoring Expert Diagnostics Tool will fail on every command.
Product Line:
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0+
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment:
Diagnostics Tool
Cause:
The Diagnostics Tool must be run with administrator access for some processes.
Resolution:
Right click on the Diagnostics Tool, and run as administrator.