Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What is the actual temperature on the heat sink if the ATV61 or ATV71 drives thermal is showing or reading 118%?
Issue:
Heat sink temperature on the ATV61/71 if thermal reading is 118%.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Wants to know how hot the heat sink is getting when the drives thermal is showing 118%

Resolution:
Approximately 100 degrees C is measred on heatsink.