How can you read over modbus if the ATV61 or ATV71 drive is in local or remote control mode with the F4 function key?
Issue:
ATV61 or ATV71 drive is in local or remote control mode with the F4 function key reading over modbus?
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to know if the F4 function key is in local or remote mode.
Resolution:
I suggested he monitor Address 8441 or 8442 bit 2 to show graphic display command or reference.
This bit 2 will go high when in local HMI mode.
Udgivet til: Schneider Electric Danmark