Hvordan kan vi hjælpe dig i dag?

Does the ATV312 have Brake Logic Control?

Issue:
Can I set up Brake Logic Control on the ATV312?

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
Customer wanted to use brake logic control function.

Resolution:
The ATV312 does have a Brake Logic Control function.  This enables the drive to manage an electromagnetic brake.
To program it, go to menu FUN, then sub-menu bLC-, then bLC (brake assignment).
See attachment, excerpt from the program manual.

Schneider Electric Danmark

Bilag
ATV312 brake locic control.pdf [162.02 KB]