Hvordan kan vi hjælpe dig i dag?

Does the M241 support Profibus?

Yes the M241 supports the Profibus protocol. The TM4PDPS1 communication module can be used to configure a slave connection on Profibus DP