Hvordan kan vi hjælpe dig i dag?

What it he maximum number of SoMachine protocol connections for a TM241 and TM251 controller?

There is a maximum of eight SoMachine protocol connections for the embedded Ethernet port of a TM241 or TM251 controller. SoMachine will use one of these connections to connect to the PLC.
This information is for controllers with a firmware version corresponding to SoMachine v4.3.