Hvordan kan vi hjælpe dig i dag?

Use the serial port 1 of Twido as Modbus port,could the program cable be used as the communication cable?

No,the communication cable connecting to serial port 1 should short pin 5 and pin 7.