What is the MTBF on the BMXNOC0401?
Issue:
What is the MTBF on the BMXNOC0401?
Product Line:
BMXNOC0401
Resolution:
The MTBF at various conditions (in hours) is presented below in this table:
| Product | MTBF 30° Continuous | MTBF 30° Intermittent | MTBF 60° Continuous | MTBF 60° Intermittent | MTBF 85° Continuous | MTBF 85° Intermittent | Nb Cpt Missing | Nb Cpt Missing * Qty | Nb Cpt Total * Qty | Ratio Nb Cpt Missing / Nb Cpt Total |
| BMXNOC0401 | 1554139.217 | 896891.553 | 908288.313 | 624804.358 | 548512.653 | 425723.762 | 1 | 8 | 390 | 2.10% |
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: