Hvordan kan vi hjælpe dig i dag?

Using the ATV61 or ATV71 drives, which communication option cards allow you to view the drive through a web page?

Issue:
Webpage access with drive.

Product Line:
Altivar 61, Altivar 71

Environment:
All models and serial numbers

Cause:
Needs an option card that allows him to view an web page.

Resolution:
There were three option cards that allow web page viewing for ATV61 and ATV71.
VW3A3310D Ethernet TCP/IP card
VW3A3316  Ethernet IP card
VW3A3320 combo Ethernet TCP/IP and IP card