Can the Altivar ATV312 Drives do single phase 110 VAC input?
Issue:
ATV312 single phase 110 VAC input
Product Line:
ATV312 Drives
Environment:
All serial numbers for ATV312 Drives
Cause:
N/A
Resolution:
No it cannot. The drive can only do 208/230 VAC single-phase on the single phase input rated drives that have the M2 suffix..