What fuse size is needed for the ATS22 CL1 CL2 control circuit?
Issue:
Looking for the fuse size needed for CL1-CL2 on ATS22 soft starts
Product line:
ATS22, Altistart 22
Resolution:
The CL1 - CL2 control voltage input should have a 1A fast acting fuse, or 1A circuit breaker for each ATS22 unit. This applies to the 120V and 230V control supplies (Q, S6 and S6U).
See attachment
Udgivet til: Schneider Electric Danmark