Hvordan kan vi hjælpe dig i dag?

What are the part numbers for the replacement cooling fans for the ATV61 and ATV71 drives?

Issue:
ATV61 and ATV71 replacement part numbers for cooling fans

Product Line:
Altivar ATV61 and ATV71 open type drives

Environment:
All

Cause:
Needs a replacement cooling fan for the ATV61 and ATV71 drives.

Resolution:
See attachments

Schneider Electric Danmark

Bilag
Frame size 2 to 8 Fan Part numbers.png [327.74 KB]
Frame size 11 to 10 Fan Part numbers.png [234.56 KB]
Frame size 3 to 15 Fan Part numbers.png [263.25 KB]