Hvordan kan vi hjælpe dig i dag?

Fallback mode in the BMEAHI0812 and the BMEAHO0412

Issue
What happen when the PLC is in STOP mode or if communication between the PLC and the HART input or output module has stopped?

Product Line
M580, BMEAHI, BMEAHO

Resolution
Please refer to the attached file.

Schneider Electric Danmark

Bilag
Fallback mode the BMEAHI0812 and the BMEAHO0412.pdf [113.2 KB]