Alternative for standard locking system for Thalassa PLD
For the installation of an alternative to the standard DIN barrel on handle from PLD enclosures by a DIN barrel with another number of key. Example of DIN barrel usable on handle from PLD enclosures - DIN barrel made by JMP Diffusion type 1327/999 - DIN barrel made by EMKA type 1109-U1-N See document in attachment.