What materials are used in the connection terminals of the LV power cables on a TRIHAL cast resin dry type transformers?
The neutral point has been standardised as a copper bar with "bimetal" washers on a TRIHAL cast resin dry type transformers. The connector plates for the phases are tinned aluminium. Consequently, "bimetal" connection terminals are not necessary for connecting the power cables.