Hvordan kan vi hjælpe dig i dag?

What is the max current for the +24v internal supply on the ATV61 drive?

Issue:
Max current for the +24v internal supply on the ATV61/71 drive.

Product Line:
All ATV61/71 drives

Environment:
+24v internal power supply on ATV61/71 drive

Resolution:
Max current for the internal +24v supply is 200mA.