Hvordan kan vi hjælpe dig i dag?

Is there a compatibility list of firmware for PL7 Micro/Premium processors?

Issue:
Is there a compatibility list of firmware for PL7 Micro/Premium processors?

Product Line:
TSXP57, TSX Premium, TSX37, TSX Micro, PL7, Firmware

Resolution:
Below is the compatibility table of firmware for the TSX Micro and Premium controllers:
TSX Micro hardware bases
---------------------------
Processor type            PV        Compatible operating systems versions

TSX3710000            =08        SV1.7
TSX3721000            =07        SV1.7
TSX3722000            =07        SV1.7

TSX3705001            <=06        SV3.5, SV4.0, SV5.0, SV5.1, SV6.0
TSX3708001            <=06        SV3.5, SV4.0, SV5.0, SV5.1, SV6.0
TSX3710001            <=08        SV3.0, SV3.5, SV4.0, SV5.0, SV5.1, SV6.0
TSX3721001            <=08        SV3.0, SV3.5, SV4.0, SV5.0, SV5.1, SV6.0
TSX3722001            <=08        SV3.0, SV3.5, SV4.0, SV5.0, SV5.1, SV6.0


TSX PREMIUM hardware bases
-----------------------------
Processor type                          PV        Compatible operating systems versions

TSX P57102                           <=08        SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8
TSX P57102                             = 10        SV4.1, SV4.2, SV4.3
TSX P57103                             = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TSX P57153                             = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TSX P57202, TSX P57252        <=08        SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8
TSX P57202, TSX P57252         = 10        SV4.1, SV4.2, SV4.3
TSX P57203, TSX P57253         = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8
TSX P572623, TSX P572823     = 01        SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TSX P57302, TSX P57352        <=08        SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8
TSX P57302, TSX P57352        = 10        SV4.1, SV4.2, SV4.3
TSX P57303, TSX P57353        = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8
TSX P573623                          = 01        SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TSX P57402, TSX P57452       <= 08       SV3.1, SV3.4, SV3.6, SV3.7, SV3.8
TSX P57402, TSX P57452         = 09       SV4.1, SV4.2, SV4.3
TSX P57453                             = 01       SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8
TSX P574823                           = 01       SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TPMX P57102                        <= 09       SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8
TPMX P57102                          = 11        SV4.1, SV4.2, SV4.3

TPMX P57202                          <= 06        SV3.1, SV3.4, SV3.6, SV3.7, SV3.8
TPMX P57202                            = 07        SV4.1, SV4.2, SV4.3

TPMX P57352                          <= 07        SV3.1, SV3.4, SV3.6, SV3.7, SV3.8
TPMX P57352                           = 08        SV4.1, SV4.2, SV4.3

TPMX P57452                         <= 07        SV3.1, SV3.4, SV3.6, SV3.7, SV3.8
TPMX P57452                           = 08        SV4.1, SV4.2, SV4.3

TPCX 571012                          <= 08        SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8

TPCX 573512                          <= 09        SV3.0, SV3.4, SV3.5, SV3.6, SV3.7, SV3.8

TPCX 57203                              = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8

TPCX 57353                              = 01        SV5.0, SV5.1, SV5.2, SV5.3, SV5.4, SV5.5, SV5.6, SV5.7, SV5.8


Examples of operating systems files:

For a TSX MICRO TSX3721001 PLC, the compatible operating systems versions are SV3.0, SV3.5, SV4.0, SV5.0, SV5.1, SV6.0.
We recommend that you use version SV6.0 contained in the TSX_372x_V60.bin file.
For a TSX PREMIUM TSX57352 PLC version PV7, the compatible operating systems are SV3.1, SV3.4, SV3.6, SV3.7, and SV3.8.
We recommend that you use version SV3.8 contained in the TSX_57352_V38.BIN file.