Hvordan kan vi hjælpe dig i dag?

The Documentation window will not come up in the ProWORX 32 software.

Issue
Documentation window will not come up

Product Line
ProWORX 32

Resolution
The ProWORX 32 Documentation window is either minimized or hidden behind another window. Close down the ProWORX 32 software. Deleted the "layout.acf" and/or "layout3.acf" file(s) from the C:\Proworx\32 folder. This resets the ProWORX 32 windows to default. Relaunch the ProWORX 32 software and the Documentation window should now reappear.