Hvordan kan vi hjælpe dig i dag?

Does the ATV312 have load sharing functionality?

Issue:
Load sharing functionality on an ATV312

Product Line:
ATV312

Environment:
All model numbers, all serial numbers

Cause:
Application requirement

Resolution:
The ATV312 does not have any Load Sharing functions. Recommend using the ATV71 or ATV930 series drives.