How to command the Altivar VFD to do a ramp stop via Modbus serial communication?
Issue:
Altivar VFD ramp stop command via Modbus serial communication
Product Line:
ATV31, ATV312, ATV61, ATV71, ATV58, ATV12, ATV32
Environment:
All serial number
Cause:
N/A
Resolution:
To command the VFD to do a ramp stop, a decimal value of 7 must be written to the command word.
Altivar VFD ramp stop command via Modbus serial communication
Product Line:
ATV31, ATV312, ATV61, ATV71, ATV58, ATV12, ATV32
Environment:
All serial number
Cause:
N/A
Resolution:
To command the VFD to do a ramp stop, a decimal value of 7 must be written to the command word.
Udgivet til: Schneider Electric Danmark