Video: How do I program and wire an ATV212 to run using 3-wire control?
Configuring Altivar 212 Drives for 3-Wire Control
Product Line:
Altivar Buildings 212
Cause:
Need to use 3-wire (momentary) control
Resolution:
Programming:
Press MODE key to AUF
Arrow down to F---, and press ENT key
Set F111 to 2
Set F112 to 49
Wiring:
Wire the F terminal from a Normally Open (NO), momentary close, START contact
Wire the R terminal from a Normally Closed (NC), momentary open, STOP contact
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Udgivet til: Schneider Electric Danmark