Issue:
TCT parameter on the Altivar process drive
Product Line:
Altivar Process
Environment:
All models, All serial numbers
Cause:
Documentation
Resoultion:
Complete Settings-> Command and Reference-> 2-wire type
From the main menu, Navigate to "Complete Settings" then "Command and Reference". From here, you can scroll down to 2/3 wire control, and if it is set to 2 wire, 2-wire control type can be found just below.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Udgivet til: Schneider Electric Danmark