Hvordan kan vi hjælpe dig i dag?

If the BME rack can be used as an extension rack in M580 system?

In future Unity v11, the BME rack will possible to be configured as an extension rack, but only X-bus is available.