How to "Move" One Variable to Another in SCADAPack Workbench (ST, FBD and LD)
Some PLC programming applications have a "move" block to perform the task of assigning one variable to another. In SCADAPack Workbench (CAM3 & CAM5) ,there are multiple programming language options as it is an IEC 61131-1 environment. Each of these languages have their unique way of performing a "move" command.
In the following examples, it is assumed you have declared local variables for each POU (Program Organization Unit)
Function Block Diagram (FBD)
Structured Text (ST)
Ladder Diagram (LD)