Hvordan kan vi hjælpe dig i dag?

Why would a drive not stop when the run command is removed?

Issue:
The drive does not stop, when the run command is removed.

Product Line:
Altivar 61, Altivar 71, Altivar 312, Altivar 212, Altivar12, Altivar 32

Environment:
All serial numbers

Cause:
The VFD is not responding to the stop command.

Resolution:
1).  Verify how the drive is receiving the stop command.
2).  Verify if the drive is programmed to get the stop command from that source.
3).  Verify the drive is not in local control.
4).  Check if the run signal is jumpered/bypassed
5).  Check to see if the motor is backfeeding voltage back into the drive.