How to wire an ATV61 or ATV71 for 2 wire control?
Issue:
Wiring an ATV61/71 for 2 wire control.
Product Line:
Altivar 61, ATV61
Environment:
All
Cause:
N/A
Resolution:
Wire connections will be between +24 and LI1. This is assuming the drive's +24 source will be used.
This is maintained contact setup.