Hvordan kan vi hjælpe dig i dag?

Is the S-Flex drive available in Nema 3R outdoor enclosure?

Issue:
Is the S-Flex drive available in Nema 3R outdoor enclosure?

Product Line:
S-Flex

Resolution:
Yes, They are available in Nema 1, Nema 12, and Nema 3R.
Nema 12 and 3R units have a longer lead time because they are not stocked and must be built to order through product selector.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.