Hvordan kan vi hjælpe dig i dag?

Why does the Analog output AO1 not deliver 10Vdc at 60 hz on ATV12 drive?

Issue:
Wondering why does the Analog output AO1 not deliver 10Vdc at 60 hz?

Product Line:
ATV12

Environment:
All

Cause:
Output is configured for Motor frequency and 0-10Vdc.

Resolution:
The tFr parameter must be set to 60 hz. The Analog output is scaled between 0 to Max Frequency (tFr).