Hvordan kan vi hjælpe dig i dag?

Does a harsh environment BMXNRP0200 exist?

Issue
Does a harsh environment BMXNRP0200 exist?

Product Line
M580

Resolution

A hardened version of the BMXNRP0200 module is not possible without a redesign, however we are able to conformal coat them.

Here are the different part numbers:

BMXNRP0200 = suitable for use in standard operating environments

BMXNRP0200C = suitable for use in standard temperature environments with pollution (gas, humidity, dust)

BMXNRP0200T = suitable for use in extreme temperature environments (-25...70 °C) with no pollution