Can a variable be assigned to the ATV32 Somove timer function block?
Issue:
Assign a Timer Function Block on an ATV32
Product Line:
Altivar 32
Environment:
Somove function block for the ATV32 all serial number
Cause:
N/A
Resolution:
No, a variable cannot be assigned to the timer function of the ATV Logic, Timer function block properties. The on and off delay time is hard set in the function block properties.
Udgivet til: Schneider Electric Danmark