Hvordan kan vi hjælpe dig i dag?

Will the new BMX redundant power supplies work with the M340?

The M340 will have the capability to use the redundant power supplies with the release of Unity V11.1 and using the BMEXBP backplanes.
It does not mean the M340 will be able to communicate on the Ethernet link - M340 backplane communications will stay BusX only. The M340
will also not have the ability to use the preventive maintanence library either.