Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
How to save a configuration to the PMESWT0100 flash memory using the DFB?
Issue

Not possible to save a configuration to the weighing module flash memory

Product Line
M580

Resolution

To save a configuration to the flash memory of the PMESWT0100 using the DFB, make sure that you ignore the DTM configuration (Ignore_DTM_configuration= 1), then set the initialization bit to 0 before saving to the flash memory (Saving_in_flash memory =1).