Hvordan kan vi hjælpe dig i dag?

Is Resi 9 electrical panel and trunking system compatible with competitors products/systems?

YES . The Resi9 electrical panels can be installed on trunking directly with Hager products and Legrand products (Gamma Hager and Legrand Drivia). Conversely Drivia and Gamma units can be installed directly on the Resi 9 trunking .
For other offers, not Schneider control panels, installation on Resi9 trunking system can be made using the universal media.
References: R9H13537 (13Modules) and R9H13541 (18 Modules)