Hvordan kan vi hjælpe dig i dag?

Upon opening Unity the DTM Catalog Update hangs at the PRM Gateway DTM.

Issue
DTM Catalog Update hangs at the PRM Gateway DTM

Product Line
M580, Quantum, Profibus Remote Master

Environment

Unity Pro

Resolution

Please install the PRM Gateway DTM V1.2.13.0.
Please use the current PRM Master and PRM Comm with this PRM Gateway DTM.

There will be a PRM Gateway DTM version 1.3 by the end of 2016 for UP11.1