Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What is the maximum available current on ATV12 Drive 24Vdc Power Supply?
Issue:
Maximum available current on ATV12 Drive 24Vdc Power Supply

Product Line:
ATV12, Altivar 12

Environment:
All

Cause:
N/A

Resolution:
Maximum customer current available is 100 mA (+ 24 VDC -15% +20% protected against short-circuits and overloads).