Hvordan kan vi hjælpe dig i dag?

What is the part number for the GT500-480 Door Switch?

Issue:
A customer would like to know the part number and specifications for the GT500-480 door switch.

Product Line:
GT500-480, GT500-600

Environment:
Installations that utilize the GT500 series inverter

Cause:
A product description and confirmation of part number is required when creating a case for a parts order.

Resolution:
The APC Part Number is 531-2017-01.
The specifications can be found below in the attachment.

Schneider Electric Danmark

Bilag
062-2017-01_SE.pdf [1.63 MB]