Hvordan kan vi hjælpe dig i dag?

Can you use one large line reactor on multiple drives vs one line reactor for one drive?

Issue:
Is it possible to use one large line reactor on multiple drives vs one line reactor for one drive?

Product Line:
Altivar Drives

Environment:
All

Cause:
Would like to use only one line reactor and feed multiple drives.

Resolution:
No, it is best to have individual line reactors. If a single line reactor is used, it will have lower inductance and may not be enough if a single drive is running.