Hvordan kan vi hjælpe dig i dag?

How do I access the embedded web page on an ATV630 drive?

Issue:
Embedded web page in an ATV630

Product Line:
ATV600 process drive including:
ATV630, ATV650, ATV660, ATV680 and APM drives

Environment:
All

Cause:
N/A

Resolution:
To connect to the embedded web page on the ATV6xx drive, you must first enter an IP address in the drive.  You may also need to enter a Subnet Mask and Gateway address per the network requirements.  Then power cycle the drive.
Connect via an ethernet cable from PC to drive. Open your web browser, then type the drives IP address in your browser. On the log in page if you have version 1.4 or lower, the ID & password are both admin. If your drive is V1.5 or higher, the ID is admin, and the password is found under Menu 8.7 in the drive.