BSH and BMH motors can work in temperature range -20°C to 40°C (more with derating). SH motors operation temperature is +5°C to 40°C (more with derating). The reason are mechanical tolerancies in bearings and the grease that does not work at low temperatures.