Hvordan kan vi hjælpe dig i dag?

What would cause the IP address to reset back to all zeros after power cycling on the ATV61 or ATV71 VW3A3327 Profinet option card?

Issue:
Why does the IP address reset back to all zeros after power cycling the ATV61/ATV71 VW3A3327 Profinet option card?

Product Line:
ATV61 and ATV71

Environment:
All

Cause:
Force to local is set

Resolution:
Check to see if force to local is turned on if so turn it off and use the ref and command switching in menu 1.6 and 1.7.