Hvordan kan vi hjælpe dig i dag?

Is the ATV660 Harmonic filter IEEE519 compliant?

Issue:
IEEE519 compliance of the ATV660 Harmonic filter.

Product Line:
ATV660

Environment:
All

Cause:
Standard compliance required

Resolution:
An ATV660 ordered with a modification M09, Harmonic filter in field 09, complies with IEEE519.
See the attached file for supporting documentation.

Schneider Electric Danmark

Bilag
ATV660 Harmonic filter.pdf [70.92 KB]