Hvordan kan vi hjælpe dig i dag?

What is the part number for the Controller Inside Card for the ATV61/71 Drives?

Issue:
Part Number for the Controller Inside Card for the ATV61/71

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
The part number is VW3A3501. See attachment for a picture of the Controller Inside Card. This is a blank, programmable card. It does not come pre-programmed.

Schneider Electric Danmark

Bilag
Controller Inside card.png [235.19 KB]