Does ICSA-15-246-02 actually apply to the M340 CPUs
Issue
Does ICSA-15-246-02 actually apply to the M340 CPUs?
If it does, which version firmware addresses the issue?
Product Line
M340
Resolution
A Schneider document is available at the vulnerability site:
http://www.schneider-electric.com/ww/en/download/document/SEVD-2015-233-01
Within the mitigation section you will find all versions this issue is fixed for each module. The CPU’s are the last in the list V4.60 IR02 for the web version and 2.9 for the firmware.