Hvordan kan vi hjælpe dig i dag?

Does the HMIG3U need a powered USB hub to power the XVGU and HMIZRA1?

Issue:
Do the XVGU and HMIZRA1 USB accessories need powered USB hubs to function with the HMIG3U?

Product Line:
Magelis HMIG3U

Resolution:
The HMIG3U does not need a powered USB hub to power the XVGU and HMIZRA1. Each of the USB ports of the HMIG3U can supply upto 500ma of current. The two devices require 400ma each