Hvordan kan vi hjælpe dig i dag?

Video: Connecting a Potentiometer to the ATV320 Drive

Issue:
Wiring a potentiometer to an ATV320

Product Line:
Altivar 320, ATV320

Cause:
Wiring and installation

Resolution:
Using the +10V source of the drive, hook up to +10, AI1, and COM.
AI1 terminal is middle (wiper) connection for a potentiometer.
+10 is the drive's 10Vdc source.
COM is neutral.