Hvordan kan vi hjælpe dig i dag?

How to Program a Delayed Off Timer using Telepace Studio?




It operates like this:
  • When Charge Pump coil (10001) is enabled by other logic in the program, Booster Pump coil (00002) is instantly latched On.
  • Whenever Charge Pump coil (10001) is turned off by other logic in the program, The T.1 timer is enabled.
  • Only after the T.1 timer counts up to its maximum (in this case 50 tenths of a second = 5 secs.), coil 100 is enabled which unlatches the Booster pump coil (00002)

Schneider Electric Danmark

Bilag
Delayed Off Timer.tpj [22.01 KB]