Hvordan kan vi hjælpe dig i dag?

How can we view the firmware version, model and serial number of PM2225 meter ?

Issue

How can we view the firmware version, model, and serial number of the PM2225 meter?

Product Line

PowerLogic™ PM2225 Series Meter.

Environment

Installations where device identification, firmware tracking, and maintenance records are required for asset management or troubleshooting.

Resolution

You can view the meter’s firmware version, model, and serial number directly from the display panel by following these steps:

  1. Navigate to Maint > Diag on the meter’s display.
  2. Press Info to view the following details:
    • Meter model
    • Serial number
    • Date of manufacturing
    • OS version
    • RS version
  3. Press Up to exit the screen.