Hvordan kan vi hjælpe dig i dag?

How to assign a fixed IP address to SmartConnect enabled Smart-UPS

Issue:
Would like it configure SmartConnect enabled Smart-UPS with a fixed IP address AKA static IP address.

Product Line:
SMTL, SCL, SMT, SMC, SMX, SRTL model Smart-UPS with embedded SmartConnect network port.

Environment:
Smart-UPS with embedded SmartConnect network port
SmartConnect link

Cause:
Informational

Solution:

For SMT with firmware 4.1 or greater and SMTL, SMX, or SRT model Smart-UPS
From the LCD panel scroll to Configuration and using the down arrow scroll to Menu Type. Set the menu type to Advanced. Then using the down arrow scroll to UPS IP Address Settings and press enter. From the UPS IP Address Setting menu you can change from DHCP to Manual and enter a static IP address, subnet mask, gateway, and DNS.
SmartConnect IP address

For SMT model with firmware less than 4.1 and all SCL, SMC models
To set a fix IP address for the embedded SmartConnect network port you must allocate an IP address to the UPS mac address or reserve an IP for the mac address via your router/DHCP server. See the router user's guide or contact your network administrator for assistance.

The mac address is the product UPS ID number. It will be found on the QR code sticker of the UPS.
QR code sticker
QR code sticker 2