Hvordan kan vi hjælpe dig i dag?

Which function can we do with the ZBRT2 wireless button ?

This product is done to do only one function set-reset, that means the output of the receiver will be active when the operator will push the button and inactive when he will release it.